Start of Interval

Associated with: Master Station Accumulators on which the total is reset on an End of Period basis

This attribute displays the date and time at which the Accumulator’s current or latest End of Period Reset interval started.

Use the attribute in conjunction with the Interval and End of Interval status attributes.


Disclaimer

Geo SCADA Expert 2019