The Effects of Suppression on Alarm Displays

The table below indicates how the alarm condition that triggers alarm suppression affects the entries in alarm displays, such as Alarms Lists and the Alarm Banner:

Parent Alarm Object Entry in Alarm Displays Child Objects Alarm Status Entries in Alarm Displays

No active alarms

---

Any alarms

Unacknowledged Uncleared/
Acknowledged Uncleared/ Unacknowledged Cleared

VISIBLE

Alarm that triggers alarm suppression raised

VISIBLE

Existing alarms that were raised pre-suppression

Unacknowledged Uncleared/ Acknowledged Uncleared

VISIBLE

Alarms that cleared pre-suppression, which remain unacknowledged

Unacknowledged Cleared

VISIBLE

Existing alarms, raised pre-suppression, which have been acknowledged while suppression is in force

Acknowledged Uncleared

VISIBLE

Alarms raised while suppression is in force

Unacknowledged Uncleared

Suppressed (not shown)

Alarms raised while suppression is in force and which have cleared while suppressed (Geo SCADA Expert automatically acknowledges any alarms that are raised then clear while still suppressed)

---

---

Alarm that triggers alarm suppression cleared

VISIBLE (Unacknowledged Cleared)/
--- (once acknowledged)

Any alarms, regardless of whether they were raised pre-, post-, or during suppression

Unacknowledged Uncleared/ Acknowledged Uncleared/ Unacknowledged Cleared

VISIBLE*

Different type of alarm raised**

VISIBLE

Any alarms, regardless of whether they were raised before or while the parent object’s alarm is active

Unacknowledged Uncleared/ Acknowledged Uncleared/ Unacknowledged Cleared

VISIBLE

* The date and time assigned to any alarms that were suppressed but become visible once suppression is no longer in force varies, depending whether the Use Visible Time As Alarm Active Time feature is enabled. If the feature is enabled, the alarm entries are time stamped with the date and time that they became visible post-suppression; if the feature is disabled (the default on most systems), the alarm entries retain their original time stamp (indicating the alarm’s original receipt time or occurrence time).

** Only some types of database item support more than one type of alarm.

Further Information

Alarm Status.

Activities that Occur when an Alarm is Raised.

Define whether the Visible Time is used as the Active Alarm Time.


Disclaimer

Geo SCADA Expert 2019