Counter-Type Points with Different Limits
            Some counter-type points have different types of alarm limit to those explained in this guide. 
Counter-type points can also be configured to have:
- Two sets of alarm limits (see Multiple Alarm Limits)
 - Multiple Point State Alarms (in which case an additional Alarm column is displayed in the Alarm Limits section of the Point Form).