Custom Configuration Fields
            You can add ‘custom’ configuration fields to the Geo SCADA Expert database—for example, you might add a custom ‘Description’ field to the points in your system.
You can include the data from such ‘custom’ fields in your reports, in the same way as other fields. Custom fields are listed in the Database Schema and are displayed alongside other Database fields in Crystal Reports’ Field Explorer Bar.
For information on configuring ‘custom’ configuration fields in Geo SCADA Expert, see Extra Database Fields in the Geo SCADA Expert Guide to Server Administration.