Custom Data Fields
            You can add ‘custom’ data fields to points in the Geo SCADA Expert database—for example, you might add a custom ‘ExportTime’ field to the points in your system, in order for an external application to assess the period for which it is to export point data.
You can include the data from such ‘custom’ fields in your reports, in the same way to other fields. Custom fields are listed in the Database Schema and are displayed alongside other Database fields in Crystal Reports’ Field Explorer Bar.
For information on configuring ‘custom’ data fields in Geo SCADA Expert, see Extra Database Fields in the Geo SCADA Expert Guide to Server Administration.