Export the Report in Adobe Acrobat Format

If Geo SCADA Expert is to export a report to Adobe Acrobat format, use the Format field on the Export Format tab to specify the Adobe Acrobat format.

When the Format is set to Adobe Acrobat, the tab displays these fields:

When you export a report in Adobe Acrobat format, a printable PDF file is generated. The file can be viewed using Adobe® Reader®.

This option does not affect the format of a report that is displayed on a Virtual ViewX client or Original WebX client (see Specify Whether a Report is to be Made Available for Display in Original WebX).


Disclaimer

Geo SCADA Expert 2019