Export the Report in Plain Text Format

If Geo SCADA Expert is to export a report in plain Text format, use the Format field on the Export Format tab to specify the Text format.

Unlike with programmatic-type text export formats, headers and footers are treated as fields, rather than data records, and as such can be used in a report that is exported to Text Format.

Be aware that the export process takes into account the report’s field widths when exporting data and truncates any content that overruns such widths.

If you want to export a report in text format for programmatic purposes, you may want to Export the Report in Separated Values Format, or Export the Report in Separated Text Format.

When the Format is set to Text, the tab displays these fields:


Disclaimer

Geo SCADA Expert 2019