Print Report

Associated with: Crystal Reports.

Security permission required to access this pick action: Control.

The Crystal Reports driver uses the server’s specified printing user when printing a report using the Print Report pick action. The printing user determines which printer(s) are available to the server. The user is specified in the Printing section of the Geo SCADA Expert Server Configuration Tool (see Printer Settings in the Geo SCADA Expert Guide to Server Administration).

Use the Print Report pick action to print a copy of a report to a printer on your system. The server produces and prints a report that contains the latest data.

The page setup for a report is specified on the Crystal Report Form (see Configure the Report Properties) and the Crystal Reports application (see Specify the Page Setup).

Select the Print Report pick action to display the Print Report window. The window displays the fields listed below. (If a report uses Parameters (see Parameter Field), other fields may be displayed, allowing you to specify the report data that is to be printed—see your system administrator for further information about such parameters).


Disclaimer

Geo SCADA Expert 2019