Preparation

You need to add a DDE Server for each server on your system with which you want to communicate using the DDE protocol.

To configure a DDE Server, you need to know the DDE Service name used by the server, and the name of the node on which it is located if it is not on the same PC as the Geo SCADA Expert database. You also need to know the read and write mechanisms that are supported by the server, along with the user name(s), password(s), and domain(s) that allow the required access to the data if Geo SCADA Expert is to access the server remotely.

You also need to establish which features are required for each DDE server. You can configure each server to use a variety of features, including alarm redirection. However, many of these features are optional and have no effect on the success of communications. The optional features include:

If the features listed above are not configured, they are not used for the selected server (they will be left blank).


Disclaimer

Geo SCADA Expert 2019