DNP3

Configure the Number of Events Required to Generate an Unsolicited Message

Use the fields within the Buffered Events section of the DNP3 tab to define the minimum number of buffered events that are required in order for Geo SCADA Expert to send an unsolicited message to the DNP3 master. When Geo SCADA Expert generates an unsolicited response, it sends the buffered events (of all enabled event classes) for the DNP3 Slave outstation to the DNP3 master.

(The Event Notification Delay field is near the top of the DNP3 tab—for information, see Configure the General DNP3 Properties.)


Disclaimer

Geo SCADA Expert 2019