DNP3

General Properties

Use the fields at the top of the Analog Point tab to define the general properties for a DNP3 analog point. The properties are common to many DNP3 points—for information, see Configure General Point Properties.

You use the Severity field shown above to define the severity of alarms and events other than those that are generated in relation to changes in the point’s state or value. You use the Severity fields within the point’s Alarm Limits section to specify the severity level(s) of state-related alarms and events (see Alarm Limits).


Disclaimer

Geo SCADA Expert 2019