DNP3

Key Wrap

The Key Wrap algorithm is the algorithm that is used to encrypt the Session Keys and Challenge Data during a Session Key Change. Devices that use DNP3 Secure Authentication have to support the Advanced Encryption Standard (AES) AES-128 algorithm. AES-128 is the algorithm that Geo SCADA Expert uses during each Session Key Change.

A pre-shared private Update Key is used in the encryption process.

Further Information

Specify the Algorithms used to Secure Message Content.


Disclaimer

Geo SCADA Expert 2019