DNP3

Protocol Alarm

Associated with: DNP3 master outstations

The Protocol Alarm attribute is common to outstations on many advanced drivers, but the errors that it might indicate differ, depending on the driver. With outstations on the DNP3 driver, the Protocol Alarm attribute might indicate that any of the following DNP3 IIN Status Bits are set at the outstation:

Possible states: Displays one of the Standard Alarm States.

Use the Protocol Alarm attribute in conjunction with the IIN Status attribute to ascertain the type of DNP3 IIN bit that is being set. Then check the Events List for any error messages that help to identify the request that is causing the IIN bit to be set. Correct the configuration in Geo SCADA Expert accordingly.


Disclaimer

Geo SCADA Expert 2019