DNP3

Specify Different Communications Parameters for an Individual Outstation

Use the fields within the Communications Parameters section of the DNP3 tab to specify whether Geo SCADA Expert is to override the default Communications Parameters that are defined for the channel (see Configure the Communications Parameters).

Enabled

Select this check box if the DNP3 communications parameters defined on the Channel Form are to be overridden by the parameters specified in this section. Select this check box and set the remaining fields if:

For the remainder of the fields within this section, see Configure the Communications Parameters.

Clear the Enabled check box if Geo SCADA Expert is to communicate with the outstation using the Communication Parameters that are specified on the Channel Form (see Configure the Communications Parameters).


Disclaimer

Geo SCADA Expert 2019