DNP3

Unsolicited Messages

Some DNP3 outstations have the capability to report event data to the DNP3 master (for instance Geo SCADA Expert) independently of that master’s polling cycles. The outstations report such event data to the master by transmitting unsolicited messages.

Use the Enable Unsolicited Messages section on the DNP3 Outstation Form to specify:

For more information, see Enable Unsolicited Message Generation.

In addition to the above, Enable Unsolicited Events and Disable Unsolicited Events pick actions can be used to enable or disable unsolicited events on an outstation, as required.

If the outstations use DNP3 Secure Authentication:

For more information on either section of the Geo SCADA Expert ServerConfiguration Tool, see Define Which Function Codes are Critical.

You can use the Unsolicited Event Reporting Status attribute to ascertain which unsolicited event classes are enabled and disabled in an outstation.


Disclaimer

Geo SCADA Expert 2019