Configure an Output Point or Pulse Action’s Interlock Properties

For each DNP3 SCADAPack Output point that Geo SCADA Expert is to control exclusively, or for which point control alters between Geo SCADA Expert and ISaGRAF, ensure that the point’s Control aggregate is enabled (see Specify Whether an Output Point is Controlled by Geo SCADA Expert in the Geo SCADA Expert Guide to the DNP3 Driver).
For each DNP3 SCADAPack Output point that is controlled exclusively by another application, rather than Geo SCADA Expert, you need to disable that point’s Control aggregate. For such points, fields on the Control tab are unavailable for use and you can ignore the rest of this section.

In addition to the properties that are common to DNP3 Output points (see Configure the DNP3-Specific Control Properties on DNP3 Output Points in the Geo SCADA Expert Guide to the DNP3 Driver), DNP3 SCADAPack Output points have the properties that are described below. The properties below also apply to DNP3 SCADAPack Pulse Actions.


Disclaimer

Geo SCADA Expert 2019