Description

Associated with: DNP3 SCADAPack Firmware Image items.

This status attribute indicates the Description that was entered for the compressed binary firmware image file when it was imported into the Geo SCADA Expert database (see Import Firmware Image).

Use this status attribute in conjunction with the File attribute to ascertain information about the .biz file with which this particular DNP3 SCADAPack Firmware Image item is associated.


Disclaimer

Geo SCADA Expert 2019