Display Trend Objects
Associated with: DNP3 SCADAPack points to which at least one Trend item is attached
Security permission required to access this pick action: Read
Use the Display Trend Objects pick action to display a Queries List of the Trend database item(s) that are associated with this particular point. Each Trend item defines the rate at which the outstation samples the point’s data (see Configuring DNP3 SCADAPack E Trend Sampler Functionality).
The Display Trend Objects pick action is not a method and therefore cannot be used with the Automation Interface.