Execute Command

Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations

Security permission required to access this pick action: Retrieve Data

Use the Execute Command pick action to execute a particular command. This section details only commands that are specific to DNP3 SCADAPack E Outstations. For further information on using the Execute Command action, see Execute Command in the Geo SCADA Expert Guide to the DNP3 Driver.

SCADAPack E outstations support the execution of a number of commands via DNP3 including:

For further information on using these commands on SCADAPack E outstations via DNP3, see the SCADAPack E Operation Reference Manual.


Disclaimer

Geo SCADA Expert 2019