Quick Start Tutorial

This section provides a guided tour designed to lead you through connecting a SCADAPack Eoutstation to Geo SCADA Expert, then communicating with that outstation using the DNP3 protocol. The procedure is for a SCADAPack ES outstation, however similar steps can be undertaken using other E outstation models.

To perform the procedure, you will need:

Now proceed as follows:

  1. Confirm that the DNP3 and SCADAPack E Server Components are Installed.
  2. Setup a SCADAPack ES Outstation.
  3. Create the Geo SCADA Expert Database Items.
  4. Power Up the SCADAPack ES Outstation.
  5. Control the DNP3 SCADAPack Analog Output Point.

Disclaimer

Geo SCADA Expert 2019