Specify the Location of the Point on the I/O Module, I/O Card, or Remote Outstation

Point data is stored in a series of point channels on each I/O module or card. Use the Channel or Remote Point Number combo box on the Mapping tab to specify the point channel that is used to store this point’s data on the I/O module or card.

If the point Mapping is to a Remote DNP3 device, you need to specify the Remote Point Number manually in the field of that name.


Disclaimer

Geo SCADA Expert 2019