Status Point for

Associated with: DNP3 SCADAPack Binary points that are configured as 5000 Series I/O Status points.

This status attribute indicates the full name (including the database path) of the DNP3 SCADAPack 5000 Series IO database item for which that binary point is the Status Point.

The attribute only applies to DNP3 SCADAPack Binary points that are configured as the Status Point on DNP3 SCADAPack 5000 Series IO database items (see Configure the 5000 Series I/O Properties). The Status Point indicates the communications status of the I/O module that the DNP3 SCADAPack 5000 Series IO database item represents.

Example:

Eastern Region.Zone 3.RTU 55 IO Module

(Indicating that the binary point is the Status Point for the DNP3 SCADAPack 5000 Series IO item ‘RTU 55 IO Module’. The 5000 Series IO database item resides in the group ‘Zone 3’, which is itself in the group ‘Eastern Region’.)


Disclaimer

Geo SCADA Expert 2019