Database Hierarchy

The Geo SCADA Expert database structure comprises a set of hierarchical Classes that contain a collection of Fields, Aggregates, and Methods. The class hierarchy defines the parent-child relationships between the classes, whereby a class can be derived from another class.

Each parent class is referred to as a Base Class, and each child class is referred to as a Sub-Class. Each sub-class inherits every one of its parent classes.

Example:

The CDBPoint class inherits the CAlarmObject and CDBObject classes.

The CAlarmObject class inherits the CDBObject class.


Disclaimer

Geo SCADA Expert 2019