Understand Configuration Change CRCs

This topic is about Configuration Change CRCs and Configuration Change Group CRCs that can be used to monitor user-instigated configuration changes. These CRCs are different to the Configuration CRCs that Geo SCADA Expert uses internally for synchronization and other purposes. (The internal Configuration CRCs are unaffected by enabling or disabling the Configuration Change CRC feature.)

Every item in the database is assigned a Configuration Change CRC value. You can enable the Configuration Change CRC feature so that this cyclic redundancy check (CRC) value is recalculated whenever the item's configuration changes. The triggers for a change in CRC value comprise any of the following:

Groups, Group Templates, and Group Instances additionally have a Configuration Change Group CRC that changes whenever that group's configuration, or the configuration of any items in that group or any sub-groups, changes (providing that the Configuration Change CRC feature is enabled). The triggers for a change in CRC value are the same as those listed for Configuration Change CRC values above.

In addition to the above, if the configuration of a Group Template changes, this will result in the Configuration Change CRC and Configuration Change Group CRC values changing in both the Group Template and the Group Instances that reference that Group Template.

Two database items of the same type, with the same name, and the same configuration (including references to other items in the database), on a system running the same version of Geo SCADA Expert, will have the same Configuration Change CRC value. The CRC values of a Group Template and its Group Instances will differ, and as such, the CRC values of a Group Template and its Group Instances are not directly comparable.

When the feature is enabled, Geo SCADA Expert uses the Configuration Change CRC and Configuration Change Group CRC values to determine whether an item or group's configuration has changed. System administrators may also find the CRC values useful for detecting whether configuration remains unchanged, such as in the following scenarios:

For more information, see Determine which Items in a Group have Changed Configuration, and see Ascertain which Configuration has Changed.

If you intend to use Configuration Change CRC values to determine whether configuration changes have occurred, remember to take a new 'snapshot' of the relevant archives, backups, or sdes whenever you upgrade your system (as various CRC values might have changed on upgrade).

If you change an item's configuration, but then change that configuration back again, the item's Configuration Change CRC value will revert back to the value that existed before the configuration change was implemented and then reverted. However, the item's Last Modified status attribute will change to show the date that the item's configuration last changed (even if that change resulted in the configuration reverting back to its previous setting).

Further Information

The Convert To feature: see Converting a Database Item in the Geo SCADA Expert Guide to Core Configuration.

Group Templates and Group Instances: see Group Templates and Group Instances in the Geo SCADA Expert Guide to Core Configuration.


Disclaimer

Geo SCADA Expert 2019