Current State

Associated with: Points

This status attribute displays a point’s current state (rather than its Current Value).

Use the attribute in conjunction with other attributes, such as Current Quality to assess the reliability of the point’s data.

(The possible states for a point are specified on a per-point basis, on the corresponding Point Form.)

Also see Previous Update State, and see Current M/S State.


Disclaimer

Geo SCADA Expert 2019