Disable Scanner
            Associated with: Scanners and Slave sources
Security permission required to access this pick action: Disable Points
                        
Use this pick action to take a scanner or Slave source Out of Service.
The Disable Scanner pick action clears the scanner or source's In Service property, so that the item is no longer active.
You might want to disable a scanner, for example, if Geo SCADA Expert has detected a problem with the devices that the scanner polls. Once the problem has been rectified, use the Enable Scanner pick action to place the item back In Service.
Geo SCADA Expert logs an entry in the Event Journal whenever either pick action is used. The entry indicates whether the scanner or Slave source has been enabled or disabled.
Be aware that disabling a scanner also de-activates the points associated with that scanner, although their configuration will remain unchanged.
If using this pick action with the Automation Interface, you need to specify the method name Disable.