Enable Server

Associated with: Servers

Security permission required to access this pick action: Disable Points

Use this pick action to place a server In Service. Triggering the action changes the server's configuration so that its In Service property is enabled. Once enabled, the server becomes active.

The Enable Server pick action is only available for a server:

Also see Disable Server.

If using this pick action with the Automation Interface, you need to specify the method name Enable.


Disclaimer

Geo SCADA Expert 2019