Extend Line

Associated with: PSTN outstations or outstations with PSTN fallback; Slave PSTN outstations

This pick action is only available on an outstation:

Use the Extend Line pick action to reset a PSTN call that is in progress, if that call is otherwise likely to terminate before Geo SCADA Expert has finished retrieving the outstation’s data. Geo SCADA Expert re-applies the outstation’s Maximum Call Length from the instant that the Extend Line action is executed. For more information, see Define an Outstation’s PSTN Properties in the Geo SCADA Expert Guide to Advanced Drivers.

Also see One Shot, and see Open Line.


Disclaimer

Geo SCADA Expert 2019