IO Logging

Associated with: Channels on advanced drivers

This status attribute indicates whether Geo SCADA Expert is logging the communications on a channel, including data that was discarded by the driver (see Communications Logging Status in the Geo SCADA Expert Guide to Server Administration).

For more information, see Communications Logging in the Geo SCADA Expert Guide to Server Administration.

Possible states:

Further Information

Enable IO Logging.

Disable IO Logging.


Disclaimer

Geo SCADA Expert 2019