Import an SSL Certificate into the Database

WARNING

POTENTIAL SECURITY BREACH

We strongly recommend using network-connected Geo SCADA Expert drivers in a private network only (either physical or virtual). We recommend against using such drivers for communications over the public Internet. If the drivers are used over the public Internet, as a minimum those drivers should use valid SSL certificates to initiate secure connections and encrypt the data that is transmitted over the network.
Failure to follow these instructions can result in death, serious injury, or equipment damage. The breach in system security could expose sensitive data and the leave the database vulnerable to unauthorized and potentially malicious use.

In order for Geo SCADA Expert to use an SSL certificate, you have to import that certificate into the database. To do this, you use the Import Certificate pick action on the relevant SSL Certificate database item (the database item that is used to store the certificate details). The dialog box that is displayed when you select the pick action varies, depending on the type of SSL Certificate database item:

NOTICE

LOSS of communication

If Geo SCADA Expert is unable to establish a network connection with a device that uses an SSL certificate, check that the certificate is valid, has not expired, and has not been revoked. Perform these checks in addition to those that you would otherwise perform if Geo SCADA Expert is unable to establish a connection with a device.
Failure to follow these instructions can result in loss of communications between Geo SCADA Expert and the network-connected device.

Disclaimer

Geo SCADA Expert 2019