Last Outgoing Call Not Established

Associated with: PSTN outstations or outstations on which PSTN fallback is enabled

This attribute displays the date and time of the last outgoing call for which communications could not be established with the outstation. The attribute is only displayed once such a call has occurred.

Example:

20/Mar/2008 16:53:21.732

Also see the Outgoing Calls attribute, which provides a summary of the outgoing calls since the statistics were last reset.


Disclaimer

Geo SCADA Expert 2019