Logged State

Associated with: Points that have logged data

This status attribute indicates the latest logged (time stamped) point state to be retrieved for a point.

If logged data is retrieved for the point, this attribute is updated whenever new logged data is retrieved, regardless of whether Geo SCADA Expert actually stores that data historically. Geo SCADA Expert only logs the data historically if the Historic feature is enabled for the point and the data meets the historic storage criteria (see Defining Historic Details for a Point in the Geo SCADA Expert Guide to Core Point Configuration).

Use this status attribute in conjunction with other Logged attributes (such as Logged Time and Logged Value).


Disclaimer

Geo SCADA Expert 2019