Message Count

Associated with: Channels on advanced drivers

This status attribute displays statistics about the success, or otherwise, of communications messages (‘data packets’) transmitted over a particular channel.

The attribute displays the number of:

If the Reset Statistics pick action has been used to reset the count, two entries are displayed—the lower entry lists the previous Message Count, the upper entry is ‘live’ and lists the Message Count since the pick action was last used. The period to which each Message Count applies is indicated by the channel’s Comms Statistics attribute.

Example:

15 messages, 13 replies, 0 unsolicited, 2 timeouts, 0 errors

13564254 messages, 13562911 replies, 55 unsolicited, 382 timeouts, 0 errors

Use the Message Count status attribute in conjunction with the channel’s Comms Statistics attribute to ascertain the time period for which each set of statistics applies.

To ascertain which of the above statistics might relate to a particular outstation on the channel, look at that outstation’s Comms Statistics status attribute. (Be aware that the outstation’s attribute statistics do not take into account which channel(s) were used to communicate with that outstation.)


Disclaimer

Geo SCADA Expert 2019