Parity

Parity is a method of error checking that is supported by some communications equipment. When supported, the ‘sending’ operating system adds an extra bit (the Parity bit) to each byte of data that it sends to the ‘receiving’ operating system.

Each byte of data contains:

Before the data is sent from the PC running Geo SCADA Expert, the PC's operating system sets the Parity bit. The setting that is applied varies according to the Parity configuration setting of the channel (which has to match the configuration supported by the communications equipment):

When the operating system has set the Parity bit, it transmits the data via the relevant Port (defined in the channel's configuration). When the intermediate device that relays the message receives the data, it performs a calculation to determine whether the setting for the Parity bit is consistent with its configuration. If it is not consistent, the data is rejected and a parity error is generated.

The Parity bit check allows the communications equipment to determine whether the received data is valid, and varies according to the Parity configuration of the channel and communications equipment.


Disclaimer

Geo SCADA Expert 2019