Previous Update Value

Associated with: Points

This status attribute displays a point’s value at the time that it was Previously Updated in Geo SCADA Expert (as opposed to its Current Value).

The Previous Update Value might be the same as the Current Value if the point’s value has not changed since the last data retrieval.

A driver typically polls and retrieves a point’s data at the rate it is configured to do so, but only sends point updates to the Geo SCADA Expert server if that point’s value has changed. In such circumstances, the Previous Update Value and Current Value will differ. The exception to this is if another activity requires the point’s value to be passed to the server, regardless of whether that point value has changed. Such an activity would include, for example:

Any of the above activities can result in the point’s Previous Update Value being identical to the Current Value.

Use the attribute in conjunction with other status attributes, such as Previous Update Quality to assess the reliability of the data.

Also see Previous Update State.


Disclaimer

Geo SCADA Expert 2019