Put Aside Value

Associated with: Points for which a local Override is currently in force

This status attribute displays the point value that was ‘put aside’ at the time that the current local Override came into force.

Use the attribute in conjunction with the other Put Aside status attributes (such as Put Aside State and Put Aside Quality) to ascertain further information about the point data that was ‘put aside’.


Disclaimer

Geo SCADA Expert 2019