ASIN

The ASIN function is a mathematical function that returns the inverse Sine (radians) of a number. The ASIN function returns a real value.

Function Name

ASIN

Description

Returns the inverse Sine (radians) of a number.

Arguments

ASIN(INTEGER or REAL)

The ASIN function can have one input and this can be either an integer or a real floating value—see Number (Integer or Real).

Returns

REAL

The inverse Sine (radians) value of the input.

Example:

ASIN(1)

The output is 1.57.


Disclaimer

Geo SCADA Expert 2019