Data Grid Expressions

If your database contains Data Grid items, you can reference their cells in expressions. You can reference an individual cell or you can reference a range of cells (an array).

Data Grid expressions do not support indirect tags.

The grammar for data grid expressions is an extension of the grammar for Standard Expressions :

<cell> <field><row>

<cell-block> <field><row> ":" <field><row>

Where:

All functions support values from single cells, but only the AVERAGE, MAX, MIN, PRODUCT, and SUM functions support values from blocks of cells.

Examples:

Referencing single cells:

DATA1 + DATA5

This calculates the sum of the values that are stored in row 1 and row 5 of the field named DATA.

 

Referencing a block of cells from the same field:

MAX(DATA1:DATA6)

This calculates the maximum value of the values that are stored in rows 1 to 6 inclusive of the field named DATA.

 

Referencing a block of cells from different fields:

AVERAGE(A1:C6)

This calculates the average value of the values that are stored in the cells between row 1 of the field named A and row 6 of the field named C. The same expression could be defined as AVERAGE(C6:A1) as Geo SCADA Expert automatically determines the range of cells, even if the last cell is defined first.

 

Be careful to avoid recursive expressions that create circular references, for example, A1 = B1 + C1, B1 = A1 + D1.

Further Information

Data Grids: see Configuring Data Grids in the Geo SCADA Expert Guide to Core Configuration.


Disclaimer

Geo SCADA Expert 2019