RAD

The RAD function is a mathematical function that converts degrees to radians. It returns a real value.

Function Name

RAD

Description

Converts degrees into radians.

Arguments

RAD(INTEGER or REAL)

The value that represents the degrees value can be an integer or a real floating value—see Number (Integer or Real).

Returns

REAL

The result is the input (in degrees) converted into radians.

Example:

RAD(180)

The output is 3.14


Disclaimer

Geo SCADA Expert 2019