Scanners Group

The FloBossDemo.sde file includes a Scanners group.

The Scanners group contains the FloBoss Scanner objects that connect the Point objects to the Channel objects.

A FloBoss Scanner’s configuration contains the unit and group addresses for the FloBoss with which it is to communicate. As such, at least one FloBoss Scanner object is required per physical FloBoss device.

As a FloBoss Scanner can only have one sampling interval and one offset, the example configuration includes multiple scanners, each with their own polling rate. They are set up as follows:

Using a single scanner on a FloBoss would be acceptable, providing that only one sampling interval and offset were required.


Disclaimer

Geo SCADA Expert 2019