Geo SCADA Expert Configuration for Hilscher Devices on PROFIBUS-FMS Systems

In order for Geo SCADA Expert to communicate with Hilscher devices on a PROFIBUS-FMS system, you need to configure:

  1. A Hilscher Board for each I/O board through which you want to scan an FMS device (see Configuring a Hilscher Board).
  2. A Hilscher Profibus FMS Scanner for each type of data that you want to scan at a different location or different scan rate on an FMS device (see Configuring a Hilscher Scanner).
  3. A Hilscher Profibus Point for each measuring instrument or control device that you want Geo SCADA Expert to monitor or control on an FMS device.

    Choose from:

    • Hilscher Profibus FMS Analog Point (for analog input or output data)
    • Hilscher Profibus FMS Digital Point (for digital input or output data).

    For more information, see Points Used on Hilscher Scanners.


Disclaimer

Geo SCADA Expert 2019