Configure Point Scaling

Use the fields within the Scaling section of the Hilscher tab to specify the range of raw input signal values for an analog point, or the scaling factor for a calculated analog value.

The Hilscher driver uses these values in calculations to convert raw input signal values into engineering values.


Disclaimer

Geo SCADA Expert 2019