Alarm Limits

Use the fields within the Alarm Limits section of the Analog Point tab to set limits for the point and specify whether an alarm or event is generated if a point exceeds those limits. For information on configuring these limits, see Configure the Limits for an Analog Point in the Geo SCADA Expert Guide to Core Point Configuration.

The Alarm Limits section of the tab also has these fields:

If the Area of Interest feature is enabled on your system, an additional Area of Interest field is displayed on the Analog Point tab. For information on this property, see Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2019