Download File

Associated with: IEC 60870-5 Outstations

Security permission required to access this pick action: Retrieve Data

Use the Download File pick action to download a binary file from the Geo SCADA Expert server to an IEC 60870-5 outstation. Select the pick action to display the Download File window. Use the fields in the window to specify the file and the destination to which it is to be downloaded.

Also see Get Directory.


Disclaimer

Geo SCADA Expert 2019