Typical Identification Values for KEMA points

The following table lists the defined data types for KEMA points and the corresponding Type Identification Values.

Type of Measurement Type Ident. Value Data type description
Analogue values 9 Measured value: normalized value
  10 As above with time tag
  11 Measured value: scaled value
  12 As above with time tag
Digital command 45 Single command
Analog command 48 Setpoint command: normalized value
  49 Setpoint command: scaled value
Digital status 1 Single point information
  2 As above with time tag
Counter values 15 Integrated total
  16 As above with time tag

Disclaimer

Geo SCADA Expert 2019