Module n

Associated with: Kingfisher outstations

Module status attributes are displayed once the outstation is or has been in communication with the server. One status attribute is displayed per outstation module, including each of the I/O modules on which points are located. Each status attribute displays information about that particular module.

Example:

Module 1 PSU-6 Power Supply Module
Module 2 CP-11 Master Processor Module
Module 3 MC-31 Multi Communications Module


Disclaimer

Geo SCADA Expert 2019