Specify the System ID

The System ID is a synchronization character that is used within the Kingfisher network. By default, the ID is 174 (AE in hexadecimal notation). If your network uses a different System ID, change the ID in the System ID field accordingly.

You can also specify a Local System ID for an outstation set or an outstation (see Specify a Local System ID (Outstation Set)) and (see Specify a Local System ID (Outstation)).


Disclaimer

Geo SCADA Expert 2019