CommentNo

Associated with: The Event Journal table (CDBEventJournal)

Geo SCADA Expert is supplied with various ‘standard’ Events Lists—the Events List for a particular system, and the Events Lists for an individual Group or database item. Each of these Lists query the Event Journal table. Users can insert a comment for any event in any of these Events Lists, in order, for example, to indicate the unusual occurrence that resulted in a particular event being logged.

With a ‘custom’ Events List, include both the SeqNo and CommentNo fields in the SELECT Clause if you want users to be able to add such comments to any entries in that List. (For information on inserting comments, see Insert a Comment for an Event.)

The CommentNo indicates the position of a comment in the sequence of comments that have been inserted for an event on an Events List.


Disclaimer

Geo SCADA Expert 2019