Preparation

ATTENTION: Any SQL queries for ‘custom’ Lists should be written by engineers who have the appropriate experience and knowledge of the SQL language. Running a badly designed SQL query can have an adverse affect on the system. All queries should include suitable restrictions to limit the number of records that are retrieved from the database. An SQL query that queries vast amounts of data will affect the performance of the server while that query executes.

In order to reference the relevant database tables and include the required data in any custom Lists:

In order to embed Lists successfully in Mimics, in addition to the above, you also need to be familiar with the principles of Mimic configuration in Geo SCADA Expert. This is covered in detail in the Geo SCADA Expert Guide to Mimics. In particular:

(Each of the above are references to sections in the Geo SCADA Expert Guide to Mimics.)

In order to add extra Table Queries successfully in Geo SCADA Expert, in addition to the bullet points listed at the start of this section, you need to be familiar with the syntax that Geo SCADA Expert supports for Table Queries (see Extra Table Queries in the Geo SCADA Expert Guide to Server Administration).


Disclaimer

Geo SCADA Expert 2019