System-Wide Events List and Event Journal Preferences

This section summarizes those Events List or Event Journal options that a system administrator can configure on a system-wide basis. Some of the options are specific to Events Lists, whereas others affect the Event Journal. Some options affect other areas of Geo SCADA Expert in addition to Events Lists or the Event Journal. Such options, if required to differ from the defaults, should be specified on each server when a Geo SCADA Expert system is first installed. The options are specified using the Geo SCADA Expert Server Configuration Tool.

You can use the Geo SCADA Expert Server Configuration Tool to:

To access a Geo SCADA Expert system, users typically log on via a User Account. Anyone who accesses the system without logging on, is logged on automatically via the Guest or Web User accounts.

Use the Root or System Group Form to define the system-wide settings for the Guest User, including:

For information on configuring either of the above, see Define the Global Settings for All Guest and Web User Accounts in the Geo SCADA Expert Guide to Security.


Disclaimer

Geo SCADA Expert 2019